August 28, 2009
The new Sinumerik 828D is the latest addition to the series of machine tool controls from the Siemens Drive Technologies Division. The new control is designed for compact class machine tools and comes with a range of sophisticated CNC functions and universal CNC programming methods. The new panel-based CNC control is precisely tailored for application in lathes and milling machines. The Sinumerik 828D is available with a horizontal and vertical control panel layout, each of which comes in two CNC performance categories.
Reference Number: IDT 200907.2015-01