Energy Sector / Fossil Power Generation
Siemens Energy, Inc., along with its consortium partner, Kvaerner North American Construction, Inc. (a subsidiary of Kvaerner ASA), achieved substantial completion of the 695 megawatt (net) supercritical pulverized coal-fired power plant located in Maidsville, West Virginia. The plant was turned over to Longview Power, LLC, which is a subsidiary of the American company, GenPower Holdings (Delaware), L.P. The Longview Plant will make a major contribution to environmentally compatible and economical power generation in the region. It is also one of the most efficient and cleanest coal-fired plants in the U.S.
"This project demonstrates that highly efficient coal-fired power plants indeed go hand in hand with low emissions and a high degree of environmental compatibility", stated Hal S. Simonds, Director of Projects, Energy Solutions - Americas at Siemens Fossil Power Generation Division. "The performance levels guaranteed by Siemens in the contract were not only maintained but were all surpassed as well". Siemens delivered an SST6-6000 steam turbine, an SGen6-3000W generator and the SPPA-T3000 control system for the Longview plant. Siemens also supplied an innovative system for air pollution control and emissions reduction for the plant which cuts emissions of dust, sulfur-dioxide, nitrous oxides and mercury, thus making a crucial contribution to cleaner coal-based power generation. The boiler for the power plant was manufactured by Foster Wheeler North America Corporation. Kvaerner North American Construction, Inc. was responsible for the construction and erection work.