Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens at UITP International Mass Transit Trade Show

Montreal, 15 May to 17 May 2017

Mobility in the age of digitalization

Visit our trade show booth at the UITP Global Public Transport Summit in the Montreal Conference Center from May 15-17, 2017. Booth SK100, Level 02.

Further Information

Siemens Mobility Division in the USA and Canada

Taking a train has become popular again over the past few years in the megacities and urban conglomerations of North America. The number of passengers is steadily increasing, as is the availability of upgraded lines. For the railway industry, the market in North America is full of potential and perspectives.

Further Information

Light rail from Siemens for San Francisco – largest US mass transit order to date

San Francisco is considered an especially environmentally friendly city. The urban environment is characterized by an extensive public transport system. In 2014, Siemens was awarded a contract by the San Francisco Municipal Transportation Agency (SFMTA) for the supply of 175 light rail vehicles of type S200 SF. One year later, SFMTA exercised its option for another 40 light rail vehicles for the public mass transit network. The trains are being built in the Siemens plant in Sacramento. Today, every third tram or light rail vehicle in the USA is made by Siemens.

Press Pictures

Siemens-built light rail vehicles ready to begin revenue service in San Francisco

In total, the company will deliver 219 light rail vehicles for San Francisco's Municipal Transportation Agency (SFMTA), Siemens' largest order for light rail cars placed in the U.S.

Siemens-built light rail vehicles ready to begin revenue service in San Francisco

The first Siemens-built light rail vehicle for San Francisco, U.S., entered revenue service. The new light rail vehicles will be built at the Siemens plant in Sacramento, California.

Siemens-built light rail vehicles ready to begin revenue service in San Francisco

The new trains include features informed by public input including a new seating configuration, new interior color schemes, and new exterior design.

Behind the scenes look at Siemens plant

215 light rail vehicles of type S200 SF are being built in the Siemens plant in Sacramento. Customer is the San Francisco Municipal Transportation Agency (SFMTA).

Proven Technology by Siemens

The S200 light rail trains for San Francisco are based on Siemens' proven S70 model, of which more than 1,300 are currently operating in North America and other regios. The two-car articulated trains can handle grades of up to 9%, reach a speed of 80.5 km/h (50 mph) and can be flexibly combined into trains of up to five cars.

Shell construction of a light rail vehicle for San Francisco

215 light rail vehicles of type S200 SF are being built in the Siemens plant in Sacramento. Customer is the San Francisco Municipal Transportation Agency (SFMTA).

215 new light rail cars for San Francisco

In January 2017, the first production Light Rail Vehicle (LRV) of the 2015 cars based on Siemens' model S200 was delivered in San Francisco.

Presentation of the full-scale LRV model along San Francisco's iconic Embarcadero

In the picture (l-r): SFMTA's director of transit John Haley, President of Siemens US Rolling Stock Michael Cahill, SFMTA's director of transportation Edward Reiskin, and the Mayor of San Francisco Ed Lee.

Full-scale LRV model along San Francisco's iconic Embarcadero

As part of this partnership, Siemens and the SFMTA recently displayed a life-size model representing a section of the light rail vehicle along San Francisco's iconic Embarcadero. The full-scale model represents design features informed by public input gathered last fall, including a new seating configuration, new interior color schemes, new exterior design and a host of other features that will improve service for hundreds of thousands of daily riders. In January 2015, San Francisco's Municipal Transportation Agency (SFMTA) has ordered an additional 40 light rail cars from Siemens for its Muni transit system. Leveraging an option under the original 175 light rail vehicle (LRV) order signed in September 2014, the 40 additional vehicles are part of the biggest Siemens order ever for light rail cars placed in the U.S.

San Francisco orders 175 light rail cars from Siemens

San Francisco's Municipal Transportation Agency (SFMTA) has awarded Siemens a contract to deliver an initial 175 light rail cars at a value of USD648 million. With an option for an additional 85 cars, this is this is one of the biggest orders for light rail cars ever placed in the USA. With this contract, Siemens secures its position as the U.S. market leader in this segment. Every third streetcar or light rail car operating in the USA today comes from Siemens. The trains will be built at the Siemens plant in Sacramento, California, and the first cars are set to be delivered the end of 2016.
In the picture: One of 3 Siemens-proposed designs, one of which will be chosen by the SFMTA following public input.

San Francisco orders 175 light rail cars from Siemens

San Francisco's Municipal Transportation Agency (SFMTA) has awarded Siemens a contract to deliver an initial 175 light rail cars at a value of USD648 million. With an option for an additional 85 cars, this is this is one of the biggest orders for light rail cars ever placed in the USA. With this contract, Siemens secures its position as the U.S. market leader in this segment. Every third streetcar or light rail car operating in the USA today comes from Siemens. The trains will be built at the Siemens plant in Sacramento, California, and the first cars are set to be delivered the end of 2016.
In the picture: One of 2 Siemens-proposed interiors currently under consideration by the SFMTA.

San Francisco orders 175 light rail cars from Siemens

San Francisco's Municipal Transportation Agency (SFMTA) has awarded Siemens a contract to deliver an initial 175 light rail cars at a value of USD648 million. With an option for an additional 85 cars, this is this is one of the biggest orders for light rail cars ever placed in the USA. With this contract, Siemens secures its position as the U.S. market leader in this segment. Every third streetcar or light rail car operating in the USA today comes from Siemens. The trains will be built at the Siemens plant in Sacramento, California, and the first cars are set to be delivered the end of 2016.
In the picture: One of 2 Siemens-proposed interiors currently under consideration by the SFMTA.

San Francisco orders 175 light rail cars from Siemens

San Francisco's Municipal Transportation Agency (SFMTA) has awarded Siemens a contract to deliver an initial 175 light rail cars at a value of USD648 million. With an option for an additional 85 cars, this is this is one of the biggest orders for light rail cars ever placed in the USA. With this contract, Siemens secures its position as the U.S. market leader in this segment. Every third streetcar or light rail car operating in the USA today comes from Siemens. The trains will be built at the Siemens plant in Sacramento, California, and the first cars are set to be delivered the end of 2016.
In the picture: 3 Siemens-proposed designs, one of which will be chosen by the SFMTA following public input.

Further Information

Siemens off-board quick-charging system for electric buses in Montreal

The achievement of national and urban climate protection goals calls for a reduction of the carbon footprint. Hybrid and electric buses are a good alternative here. Siemens offers public utilities, operators and communities a powerful complete solution which has been specially developed for urban line operation of electric buses.
As part of Montreal's "City Mobility" project, Siemens is supplying two quick-charging stations for the Monk bus route. These will provide energy to three fully electric buses from Nova (Volvo Group).
For Montreal, the City Mobility project means the installation of two high-power-charging stations along the 36 – Monk bus route to operate three fully electric Nova buses (Volvo group).

Further Information

63 light rail trains from Siemens for Calgary in Canada

Calgary is the third largest city in Canada, and its light rail system is the busiest in North America and the second-busiest in the world. The fleet consists exclusively of Siemens vehicles. A total of 156 light rail vehicles are in operation in Calgary. In 2013, Calgary awarded Siemens an order for the supply of another 63 light rail vehicles of the newer type S200. Passenger service started in July 2016.

City of Calgary orders 60 LRVs from Siemens

The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The LRVs will be built at the Siemens factory in Sacramento, USA and are due to be delivered starting in summer 2015. The full order is to be completed by December 2016. This is the first order for the new light rail generation from Siemens. The vehicles have been designed especially for the harsh climate conditions typical for Canada.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The LRVs will be built at the Siemens factory in Sacramento, USA and are due to be delivered starting in summer 2015. The full order is to be completed by December 2016. This is the first order for the new light rail generation from Siemens. The vehicles have been designed especially for the harsh climate conditions typical for Canada.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The S200 LRVs have eight doors that allow barrier-free access for wheelchair users and passengers with baby carriages or bikes. The vehicles are produced at the Siemens factory in Sacramento where around 80 percent of the electricity required in production is supplied by a two-megawatt photovoltaic plant. This helps to save about 1,470 tonnes of carbon dioxide every year.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The S200 LRVs have eight doors that allow barrier-free access for wheelchair users and passengers with baby carriages or bikes. The vehicles are produced at the Siemens factory in Sacramento where around 80 percent of the electricity required in production is supplied by a two-megawatt photovoltaic plant. This helps to save about 1,470 tonnes of carbon dioxide every year.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The S200 LRVs have eight doors that allow barrier-free access for wheelchair users and passengers with baby carriages or bikes. The vehicles are produced at the Siemens factory in Sacramento where around 80 percent of the electricity required in production is supplied by a two-megawatt photovoltaic plant. This helps to save about 1,470 tonnes of carbon dioxide every year.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The S200 LRVs have eight doors that allow barrier-free access for wheelchair users and passengers with baby carriages or bikes. The vehicles are produced at the Siemens factory in Sacramento where around 80 percent of the electricity required in production is supplied by a two-megawatt photovoltaic plant. This helps to save about 1,470 tonnes of carbon dioxide every year.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The S200 LRVs have eight doors that allow barrier-free access for wheelchair users and passengers with baby carriages or bikes. The vehicles are produced at the Siemens factory in Sacramento where around 80 percent of the electricity required in production is supplied by a two-megawatt photovoltaic plant. This helps to save about 1,470 tonnes of carbon dioxide every year.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The vehicles have been designed especially for the harsh climate conditions typical for Canada. The coupler heaters ensure the vehicles can operate in ice and snow. Cables and connectors have been dimensioned so that they withstand the extreme weather conditions. The electrically heated windshield, triple-pane side windows with low solar transmittance and improved insulation reduce thermal losses by more than 20 percent compared to previous models. This also results in reduced power consumption. Energy-saving operation of the S200 LRVs is ensured by the weight-reduced propulsion system that allows the recovery of braking energy as well as by the LED lighting that requires up to 40 percent less energy than conventional fluorescent lighting.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The vehicles have been designed especially for the harsh climate conditions typical for Canada. The coupler heaters ensure the vehicles can operate in ice and snow. Cables and connectors have been dimensioned so that they withstand the extreme weather conditions. The electrically heated windshield, triple-pane side windows with low solar transmittance and improved insulation reduce thermal losses by more than 20 percent compared to previous models. This also results in reduced power consumption. Energy-saving operation of the S200 LRVs is ensured by the weight-reduced propulsion system that allows the recovery of braking energy as well as by the LED lighting that requires up to 40 percent less energy than conventional fluorescent lighting.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The vehicles have been designed especially for the harsh climate conditions typical for Canada. The coupler heaters ensure the vehicles can operate in ice and snow. Cables and connectors have been dimensioned so that they withstand the extreme weather conditions. The electrically heated windshield, triple-pane side windows with low solar transmittance and improved insulation reduce thermal losses by more than 20 percent compared to previous models. This also results in reduced power consumption. Energy-saving operation of the S200 LRVs is ensured by the weight-reduced propulsion system that allows the recovery of braking energy as well as by the LED lighting that requires up to 40 percent less energy than conventional fluorescent lighting.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The vehicles have been designed especially for the harsh climate conditions typical for Canada. The coupler heaters ensure the vehicles can operate in ice and snow. Cables and connectors have been dimensioned so that they withstand the extreme weather conditions. The electrically heated windshield, triple-pane side windows with low solar transmittance and improved insulation reduce thermal losses by more than 20 percent compared to previous models. This also results in reduced power consumption. Energy-saving operation of the S200 LRVs is ensured by the weight-reduced propulsion system that allows the recovery of braking energy as well as by the LED lighting that requires up to 40 percent less energy than conventional fluorescent lighting.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The vehicles have been designed especially for the harsh climate conditions typical for Canada. The coupler heaters ensure the vehicles can operate in ice and snow. Cables and connectors have been dimensioned so that they withstand the extreme weather conditions. The electrically heated windshield, triple-pane side windows with low solar transmittance and improved insulation reduce thermal losses by more than 20 percent compared to previous models. This also results in reduced power consumption. Energy-saving operation of the S200 LRVs is ensured by the weight-reduced propulsion system that allows the recovery of braking energy as well as by the LED lighting that requires up to 40 percent less energy than conventional fluorescent lighting.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The vehicles have been designed especially for the harsh climate conditions typical for Canada. The coupler heaters ensure the vehicles can operate in ice and snow. Cables and connectors have been dimensioned so that they withstand the extreme weather conditions. The electrically heated windshield, triple-pane side windows with low solar transmittance and improved insulation reduce thermal losses by more than 20 percent compared to previous models. This also results in reduced power consumption. Energy-saving operation of the S200 LRVs is ensured by the weight-reduced propulsion system that allows the recovery of braking energy as well as by the LED lighting that requires up to 40 percent less energy than conventional fluorescent lighting.
The Canadian city of Calgary has awarded Siemens an order to supply 60 S200 light rail vehicles, worth more than 135 million Euros. The vehicles have been designed especially for the harsh climate conditions typical for Canada. The coupler heaters ensure the vehicles can operate in ice and snow. Cables and connectors have been dimensioned so that they withstand the extreme weather conditions. The electrically heated windshield, triple-pane side windows with low solar transmittance and improved insulation reduce thermal losses by more than 20 percent compared to previous models. This also results in reduced power consumption. Energy-saving operation of the S200 LRVs is ensured by the weight-reduced propulsion system that allows the recovery of braking energy as well as by the LED lighting that requires up to 40 percent less energy than conventional fluorescent lighting.

Further Information

Amtrak: Mainline passenger transport in the USA with rolling stock, trackside equipment and service from Siemens

Amtrak, the passenger transit company that operates in the United States and in Canadian cities close to the border, is officially called the National Railroad Passenger Corporation. However, the brand is widely known as Amtrak, a combination of the words "America" and "track". In order to upgrade mainline traffic in the busy northeastern corridor between Washington, New York and Boston and to replace old locomotives, Amtrak ordered 70 electric locomotives from Siemens in October 2010. The first of them have been in service since February 2014 with up to 18-car trains in this corridor. The last locomotives from this order were supplied in 2016. In September 2014, Siemens received the order to cover the maintenance of the locomotives for 15 years.
For the regional passenger services operated by Amtrak in several rail corridors in the United States, the Departments of Transportation of Illinois, Michigan, Missouri, California and Washington as well as the Maryland Transit Administration (MARC) placed orders in 2014 and 2015 with Siemens for a total of 81 high-performance diesel locomotives of the Charger SC-44 type.
In 2014, Siemens received the order from Amtrak to install a new Sitras SFC plus static frequency converter for the traction power supply feed-in point in the Metuchen district of Edison, New Jersey. The power converter station in Metuchen is currently being commissioned. The work is scheduled for completion by mid-2017.

Rollout of first electric locomotive for Amtrak

The first "Amtrak Cities Sprinter" type electric locomotive for our customer Amtrak has just rolled out of the manufacturing plant. The U.S. intercity passenger rail service had placed a €338 million ($466 million) order with Siemens for 70 electric locomotives in October 2010. By securing this order, Siemens has succeeded in selling its locomotives to the American market for the first time. The first units will be field tested this summer for entry into revenue service in the fall. The last of these units are due to be handed over to Amtrak as of the end of 2015. The picture shows: Joseph Boardman, Amtrak president and CEO.
The first "Amtrak Cities Sprinter" type electric locomotive for our customer Amtrak has just rolled out of the manufacturing plant. The U.S. intercity passenger rail service had placed a €338 million ($466 million) order with Siemens for 70 electric locomotives in October 2010. By securing this order, Siemens has succeeded in selling its locomotives to the American market for the first time. The first units will be field tested this summer for entry into revenue service in the fall. The last of these units are due to be handed over to Amtrak as of the end of 2015. The picture shows: Joseph Boardman, Amtrak president and CEO, and Michael Cahill, president of Siemens Rail Systems Division in the U.S. (l-r).
The first "Amtrak Cities Sprinter" type electric locomotive for our customer Amtrak has just rolled out of the manufacturing plant. The U.S. intercity passenger rail service had placed a €338 million ($466 million) order with Siemens for 70 electric locomotives in October 2010. By securing this order, Siemens has succeeded in selling its locomotives to the American market for the first time. The first units will be field tested this summer for entry into revenue service in the fall. The last of these units are due to be handed over to Amtrak as of the end of 2015. The picture shows: Joseph Boardman, Amtrak president and CEO, and Michael Cahill, president of Siemens Rail Systems Division in the U.S. (l-r).
The first "Amtrak Cities Sprinter" type electric locomotive for our customer Amtrak has just rolled out of the manufacturing plant. The U.S. intercity passenger rail service had placed a €338 million ($466 million) order with Siemens for 70 electric locomotives in October 2010. By securing this order, Siemens has succeeded in selling its locomotives to the American market for the first time. The first units will be field tested this summer for entry into revenue service in the fall. The last of these units are due to be handed over to Amtrak as of the end of 2015.
The first "Amtrak Cities Sprinter" type electric locomotive for our customer Amtrak has just rolled out of the manufacturing plant. The U.S. intercity passenger rail service had placed a €338 million ($466 million) order with Siemens for 70 electric locomotives in October 2010. By securing this order, Siemens has succeeded in selling its locomotives to the American market for the first time. The first units will be field tested this summer for entry into revenue service in the fall. The last of these units are due to be handed over to Amtrak as of the end of 2015.
The first "Amtrak Cities Sprinter" type electric locomotive for our customer Amtrak has just rolled out of the manufacturing plant. The U.S. intercity passenger rail service had placed a €338 million ($466 million) order with Siemens for 70 electric locomotives in October 2010. By securing this order, Siemens has succeeded in selling its locomotives to the American market for the first time. The first units will be field tested this summer for entry into revenue service in the fall. The last of these units are due to be handed over to Amtrak as of the end of 2015.
The first "Amtrak Cities Sprinter" type electric locomotive for our customer Amtrak has just rolled out of the manufacturing plant. The U.S. intercity passenger rail service had placed a €338 million ($466 million) order with Siemens for 70 electric locomotives in October 2010. By securing this order, Siemens has succeeded in selling its locomotives to the American market for the first time. The first units will be field tested this summer for entry into revenue service in the fall. The last of these units are due to be handed over to Amtrak as of the end of 2015.

Further Information

Charger: Most environmentally friendly diesel locomotive for high-speed transportation in the USA

In 2014, the Departments of Transportation of California, Illinois and Maryland ordered an initial lot of 34 Charger locomotives from Siemens, with an option for a total of 222 locomotives. Due to orders from other states as well as by the private rail operator All Aboard Florida, the total number of Chargers ordered amounts to 81. The locomotives are deployed in corridors of the US states, including by Caltrains (California) as Amtrak Pacific Surfliner, in Washington as Amtrak Cascades and in Maryland with the regional network operator MARC. Under the "Brightline" brand, ten Chargers are being deployed in high-speed rail services between Miami and West Palm Beach; Orlando is due to follow at a later date.

Press Pictures

Most environmentally friendly diesel locomotive for high-speed transport in the USA

In 2014, the Departments of Transportation of California, Illinois and Maryland ordered an initial lot of 34 Charger locomotives from Siemens, with an option for a total of 222 locomotives. Due to orders from other states as well as by the private rail operator All Aboard Florida, the total number of Chargers ordered amounts to 81.

On tour deployed in corridors of the U.S.

The locomotives are deployed in corridors of the U.S., including Illinois (in the picture), by Caltran (California) as Amtrak Pacific Surfliner, in Washington as Amtrak Cascades and in Maryland with the regional network operator MARC.

Strong performance for the U.S.

The Charger locomotive reaches a tractive effort on starting of 290 kN with a weight of around 120 tons. The Cummins QSK95 diesel engine is 4,400 hp-rated. These U.S. locomotives are based technically on the Siemens Eurosprinter, Eurorunner and Vectron locomotive platforms.

Further Information

Brightline: Siemens trains provide comfortable travel between Florida's cities

The first high-speed route is being built in Florida. The opening of the route from Miami to Orlando via Fort Lauderdale is scheduled for mid-2017. The trains for this project were ordered by All Aboard Florida (under the Brightline brand) from Siemens in 2014.
Since 2012, a private company has been planning and developing a high-speed intercity line in the United States for the first time in decades. On the Florida East Coast Railway route, up to 16 train pairs are scheduled to run from Miami Central via Fort Lauderdale to West Palm Beach every day. The five four-car trains with two Charger locomotives are being built in the Siemens plant in Sacramento, California. Siemens will provide service and maintenance for the Brightline trains for a period of 30 years.

Press Picture

Brightline – comfortable travel between Florida's cities

Since 2012, a private company has been planning and developing a high-speed intercity line in the United States for the first time in decades. On the Florida East Coast Railway route, up to 16 train pairs are scheduled to run from Miami Central via Fort Lauderdale to West Palm Beach every day.

Further Information

Contact

Ellen Schramke

Siemens Mobility GmbH

+49 (30) 386-22370