1. Home

NX

Fibersim

Fibersim is a specialized software solution used in industries that rely on composite materials to design, simulate, and manufacture composite structures more efficiently and accurately.

Zoomed in visual of composite material, carbon fiber weave

Why Fibersim?

Fibersim enables part-specific design approaches for advanced composite structures. These approaches are specialized depending on the industry, whether automotive, aerospace, energy, or others where composites play a role.

To be fully optimized, advanced composite parts require unique analysis, design and manufacturing workflows. Fibersim leads the industry in supporting specialized workflows for the development of advanced composites. It supports concurrent engineering where analysis and design are performed in the context of the manufacturing, which is key to developing the highest performance, lowest cost designs.

Advanced composites undergo extensive analysis and design iterations carefully considering a part’s unique weight implications. Fibersim features tight integration with Simcenter and other CAE systems, providing bi-directional updates between designers and analysts while taking manufacturing constraints into consideration.

Design for advanced composite manufacturing is available as well. Whether the manufacturing process is hand laid, tape laid, fiber placed, or braided, Fibersim has the capabilities to ensure the design is fully manufacturable before design release.

The open, multi-CAD architecture of Fibersim provides these specialized engineering capabilities in NX, CATIA and CREO. Fibersim also saves the detailed laminate structure of the composite design into Teamcenter to share across the enterprise.

Fibersim design and analysis features

Fibersim design and manufacturing features

Related resources

Reducing time-to-market with the smart biosphere application by 72 percent
Case Study

Reducing time-to-market with the smart biosphere application by 72 percent

Biosphere Foundation uses Insights Hub and Mendix to monitor and restore nature and address the climate emergency

Automotive manufacturer increases throughput by 15 percent in paint shop
Case Study

Automotive manufacturer increases throughput by 15 percent in paint shop

MGI uses Insights Hub and Plant Simulation IoT data analytics to identify the root cause of production loss

Finnish fish producer optimizes production with Insights Hub, the industrial IoT solution from Siemens
Case Study

Finnish fish producer optimizes production with Insights Hub, the industrial IoT solution from Siemens

Heimon Kala uses Insights Hub to increase production by 25 percent

Explore NX CAD products