中文 | Deutsch | Español | Français | Italiano
Site Map | Index | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
Products
Industrial Ethernet
PROFINET
Industrial Wireless Communication
PROFIBUS
AS-Interface
SINAUT
Network transitions
IWLAN/PB Link PN IO
IE/PB Link PN IO
IE/AS-i LINK PN IO
DP/AS-i LINK Advanced
DP/ASI link 20E
DP/PA link
Solutions
References
Partner

Network transitions

Network transitions between Industrial Ethernet, PROFIBUS, AS-Interface or EIB are implemented using links,PLCs or PCs. In the last two cases,integral interfaces and communications processors (CPs)can be used for the network transition.

Network transitions implemented using a link pass on the data from one network to the next without further processing. These network transitions are the DP/PA link, the DP/PA coupler, the IE/PB link, the DP/EIB link or the DP/AS-Interface for transitions between the EIB, AS-Interface, PROFIBUS and Industrial Ethernet networks.

Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use