The following table provides an overview of the composition of the various standing committees of the Supervisory Board. Click the individual designations to find out more about the committees' work.
| Members of the Supervisory Board | Chairman's committee | Audit committee | Compliance committee | Mediation committee | Finance- and Investment committee | Nominating committee |
|---|---|---|---|---|---|---|
| Dr. Gerhard Cromme* | ||||||
| Dr. Josef Ackermann | ||||||
| Lothar Adler | ||||||
| Gerd von Brandenstein | ||||||
| Dr. Hans Michael Gaul* | ||||||
| Bettina Haller | ||||||
| Berthold Huber | ||||||
| Dr. Nicola Leibinger-Kammüller | ||||||
| Harald Kern | ||||||
| Jürgen Kerner | ||||||
| Gérard Mestrallet | ||||||
| Birgit Steinborn | ||||||
| Sibylle Wankel | ||||||
| Werner Wenning | ||||||
| * Audit Committee financial expert pursuant to the Sarbanes-Oxley Act | ||||||
The Chairman’s Committee comprises the Chairman and Deputy Chairmen of the Supervisory Board as well as one further member to be elected by the Supervisory Board and performs the collective tasks of a nominating, compensation and corporate governance committee to the extent that these tasks are not performed by the Nominating Committee or, as required by German law, to be performed by the Supervisory Board in full session. In particular, it makes proposals regarding the appointment of Managing Board members, handles contracts with members of the Managing Board and prepares resolutions for the Supervisory Board in full session with respect to the compensation of the members of the Managing Board and the review of the Managing Board compensation system.
The Audit Committee comprises the Chairman of the Supervisory Board, two of the Supervisory Board’s shareholder representatives and three of the Supervisory Board’s employee representatives. As required by German law, the Audit Committee must include at least one independent member of the Supervisory Board who has knowledge and experience in the application of accounting principles or the auditing of financial statements. The Audit Committee oversees the accounting process. Together with the independent auditors, it also reviews the Company ’s financial statements prepared quarterly, half-yearly and annually by the Managing Board. On the basis of the independent auditors’ report on the annual financial statements, the Audit Committee makes a recommendation to the Supervisory Board whether or not it should approve those financial statements. It concerns itself with the company ’s risk monitoring system and oversees the effectiveness of the internal control system, in particular as it relates to financial reporting, the risk management system and the internal audit system. The internal corporate audit unit reports regularly to the Audit Committee. In addition, the Audit Committee monitors the independent audit of financial statements, in particular the independence and qualifications of the independent auditors as well as the independent auditors’ services, and performs the other functions assigned to it under the SOA.
The Compliance Committee, which was established in April 2007, comprises the Chairman of the Supervisory Board, two of the Supervisory Board’s shareholder representatives and three of the Supervisory Board’s employee representatives. The Compliance Committee monitors the Company ’s adherence to statutory provisions, official regulations and internal Company policies.
The Mediation Committee, comprising the Chairman of the Supervisory Board, the First Deputy Chairman (who is elected in accordance with the German Codetermination Act), one of the Supervisory Board’s shareholder representatives and one of the Supervisory Board’s employee representatives, submits proposals to the Supervisory Board in the event that the Supervisory Board cannot reach the two-thirds majority required to appoint a Managing Board member.
The Nominating Committee, which comprises the Chairman and the Second Deputy Chairman of the Supervisory Board as well as two further shareholder representatives, is responsible for making recommendations to the Supervisory Board’s shareholder representatives on the shareholder candidates for election to the Supervisory Board by the Annual Shareholders’ Meeting.