Technology for the Environment – Facts and Forecasts
The Sources of Greenhouse Gases
About one third of the approximately 40 billion tons of CO2e that are emitted annually around the world as greenhouse gases comes from agriculture, forestry, land clearing measures and waste. "CO2e" refers to CO2 equivalents. Other greenhouse gases –including methane, laughing gas, fluorocarbons and industrial gases (e.g. sulfur hexafluoride) –are converted into these equivalents to show their global warming potential compared to carbon dioxide (CO2). Methane’s global warming potential, for example, is 21 times that of CO2, with one ton of methane corresponding to 21 tons of CO2e. More than two-thirds of the greenhouse gas emissions (currently about 27 billion tons of CO2e) are energy-related, meaning they are caused by people’s energy consumption. The emissions result from electricity generation in power plants, generation of heat, and fuel combustion by transport vehicles. In Germany, about 87 % of greenhouse gases result from energy use, while the remaining 13 % come from other sources, including agriculture and the chemicals industry.
Power plants are the source of nearly 25 % of the world’s greenhouse gas emissions. The largest share of CO2 from these plants results from turning fossil fuels into usable energy such as electricity and district heating; a small share is also generated during the facilities’ construction and by the supply of fuels. The cumulative CO2 emissions of lignite power plants, for example, are about 1,000 g/kWh of electricity; hard coal plants produce 780 g/kWh.
And the atmosphere even feels the effect of nuclear power plants, which give off small amounts (around 25 g/kWh) of CO2 from uranium mining and enrichment. Photovoltaic facilities account for about 100 g/kWh of CO2, due to the production of solar cells, modules and inverters. Wind plants (20 g/kWh) and hydroelectric facilities (4 g/kWh), by contrast, have very low CO2 emissions.
A look at regional distribution of energy-related emissions shows the biggest shares are from the U.S. (over 21 %) and China (almost 18 %), followed by Russia (nearly 6 %), Japan (4.5 %), India (4 %), and Germany (3.2 %). According to the IEA, energy-related emissions will rise by almost 50 % to about 40 billion tons of CO2 by 2030 if countermeasures aren’t taken. As the world’s largest coal consumer, China is expected to surpass the U.S. as the largest producer of CO2 by 2010. But China’s emissions are still low, seen on a per capita basis: about four tons of CO2 per year, compared to roughly ten tons in Germany and 20 tons in the U.S.
Sylvia Trage