Elements of Life – Wastewater Purification
Cannibals, Porous Fibers and Purity
Although pollutants in wastewater are becoming increasingly complex, higher quality is also being demanded of purified water. Specialists at Water Technologies, a Siemens business unit, and at Siemens Corporate Technology have come up with new methods for purifying water more effectively while cutting costs.
Boston’s Deer Island water treatment plant uses processes from Siemens Water Technologies
Practically every household sends an unappetizing mixture of organic materials into the sewer system. The food industry contributes grease, flour, whey and cleansing agents; industrial wastewater often contains chemicals; and rainwater washes dirt into gutters—all of which adds up to an enormous challenge for wastewater treatment plants. Furthermore, stricter environmental standards and increased awareness of health issues are driving demand for better treatment solutions. Water treatment facilities are expected to remove complex pollutants, be inexpensive to run, take up little space and generate minimal hazardous waste.
The most advanced facilities use developments from Siemens Water Technologies such as MemJet—an innovative membrane bioreactor—and the "Cannibal" process—a purely biological process that substantially reduces the quantity of sludge produced by the treatment process.
Sludge mainly consists of the remains of the bacteria used for the treatment process. Depending on the level of pollutants and pathogens in the dry sludge, it can either be used as agricultural fertilizer or sent to a landfill for disposal. "The cost of sludge handling, transport and disposal has risen sharply in recent years," says Betty-Ann Curtis, Director of Biological Processes at Water Technologies Envirex Products in Waukesha, Wisconsin.
Ravenous Bacteria. The Cannibal process introduced by Water Technologies, however, allows the total amount of sludge to be drastically reduced—by 90 to 95 percent compared to conventional methods. The process utilizes the ravenous hunger of various types of bacteria to thoroughly break down the organic components of wastewater. Its end products are nothing more than water and carbon dioxide (see graphic). The sludge that accumulates in a clarifier is first pumped into a special facility where non-biodegradable or not readily biodegradable constituents such as hair, trash, grit and inert material are separated out using fine screens and a hydrocyclone. This—for the bacteria indigestible—residue is easily disposed of at local landfills.
With the acquisition of USFilter in August, 2004, the leading producer of water processing and treatment facilities in North America, Siemens has gained a highly competitive position in membrane, UV, and ozone technologies, as well as 1,500 patents that will help it provide even better products and services for industrial and municipal customers. The new business unit, which will be known as "Water Technologies," is now a part of Siemens Industrial Solutions and Services (I&S).
Most of the remaining sludge is returned to aeration basins, while the rest is pumped into a sidestream bioreactor. There, the supply of oxygen is limited in order to kill the aerobic bacteria but allow the facultative anaerobic bacteria to multiply. "These bacteria are microbes that consume oxygen when it’s available but can do without it if need be," explains Curtis. In the Cannibal tanks, the facultative anaerobic bacteria then consume the remains of the aerobic bacteria. The contents are then gradually pumped back into the aeration basins. In this environment, the aerobic bacteria gain the upper hand, growing faster than the facultative bacteria, which slowly die. "The result is a steady-state balance between growth and destruction," explains Curtis.
The amount of bacteria in the plant thus remains constant and there is no accumulation of sludge. Nevertheless, the entire facility is cleaned out occasionally since some of the particulates cannot be removed by the solids separation module. In a typical facility, which treats 5.6 million liters of wastewater per day (for a population equivalent to about 15,000 U.S. residents) the new system could save up to $300,000 a year. The Cannibal process, which is now installed at some 25 facilities in the U.S., can be easily added to existing wastewater treatment facilities, thus increasing their capacitiy.
In recent years, the trend has been to separate solids from the water with the help of membranes, rather than relying on gravity in a clarifier. These membranes are generally located in the aeration basin itself, thus obviating the final clarifier. Whereas in a conventional plant only those bacteria that quickly settle on the bottom of the clarifier are allowed to multiply in the aeration basins, membrane bioreactors can use the bacteria that are most effective at purifying wastewater. "The biological treatment process can be optimized without worrying about settleability," says Edward Jordan, Vice President of Water Technologies Memcor Products.
In a wastewater treatment plant, the purification process takes place in several steps. The most important part of the facility is the aeration basin (1). This tank is teeming with bacteria that rapidly decompose the biodegradable constituents of the wastewater when oxygen is added. In the next step of the process, the clarifier (2), solid particles settle to the floor as sludge and purified water can be returned to the environment. Until now, a large proportion of the sludge had to be disposed of at great expense in landfill sites.
This is no longer necessary, thanks to Siemens’ Cannibal process. In this process, non-biodegradable components are first removed (3) before part of the bacteria are returned to the aeration tank and the remainder are pumped into an oxygen-free digestion tower or bioreactor. There, facultative anaerobic bacteria—which can survive in an anaerobic environment—consume the remains of their aerobic relations. Once this process is completed, they are pumped back into the the aeration tank, where they die off while the aerobic bacteria thrive. The result is a 90 to 95 % reduction in sludge—most of which has been converted into carbon dioxide and water thanks to the different types of bacteria.
Due to their design, membrane bioreactors produce much less sludge than conventional facilities. In addition, they’re compact, can handle high levels of solids, and produce high-quality water. "Membrane bioreactors do have a problem with fouling, however," says Jordan. Solid organic and inorganic particles in the wastewater accumulate on the membrane’s surface, creating an impermeable layer. When that happens, more energy must be used to draw the water into the interior through areas that haven’t yet been affected. Eventually, the membrane has to be cleaned using chlorine or jets of steam.
Siemens’ MemJet process employs an elegant solution to deal with the problem of fouling. Since the membranes consist of bundles of hollow fibers, the wastewater is led along the fibers’ exterior together with a jet of air bubbles. As in other membrane systems, the interiors of the fibers hold a vacuum that sucks the water molecules into the fibers through tiny pores. Dirt particles, viruses and bacteria are left outside. The air bubbles take the solids along and prevent them from accumulating on the membrane. The bubbles also create a uniform flow along the membrane’s surface, preventing "dead spots" that are particularly susceptible to fouling. Thanks to this solution, MemJet tanks need to be chemically cleaned only once or twice a year. Ten such facilities are now in operation in the U.S., with others on the way.
Mini Treatment Plant. Since membrane technology has recently become far more affordable and water in the U.S. is increasingly being reused right after treatment, the trend is toward small, decentralized facilities. "These plants are being built where the water is needed—near irrigated fields or golf courses, for example," says Jordan. The satellite plants are connected to a municipal sewer line and consist only of an aeration tank, a membrane tank and a disinfecting facility. The extracted solids are fed back into the drain, where they are washed back to the central wastewater treatment plant. Plant operation is largely automatic, and such facilities need to be inspected only once or twice a week. According to Jordan, the satellite plants can be set up even in densely populated areas since they produce no unpleasant odors. What’s more, the small tanks are inconspicuous and are often not even recognizable.
Catching water pollutants. Siemens’ MemJet process (left) keeps membrane filters from becoming clogged. A Siemens Mewaprev facility (right) can remove metal ions from electroplating wastewater. In the future, an analysis chip (center) will enable the process to be completely automated
Membranes are also suitable for treating industrial wastewater, which often contains substances that conventional sewage systems can’t handle, such as mineral oils, salts or heavy metals. Industrial wastewater is thus often pretreated at company plants before it reaches the sewage system. As part of the EU-sponsored Mewaprev (Metal Waste Prevention) project, Frank Walachowicz and his team of engineers at Siemens Corporate Technology in Berlin have developed a solution for wastewater from the electroplating industry. Electroplating involves the application of a thin layer of metal to a plastic or metal surface. It is used to enhance vehicle parts, cell phone housings and jewelry. "These companies’ wastewater contains all kinds of metallic salts, particularly salts of copper, nickel, chromium and precious metals," says Walachowicz. Although the concentration of metals in such wastewater is sometimes as high as that found in ore deposits, the metal could, until recently, not be economically recycled.
Precious Metals from Wastewater. With the new Siemens method, however, metal ions can be inexpensively extracted from wastewater. The system’s core component is a hollow fiber module. The wastewater flows past the exterior of these fibers, while a second liquid known as a "strip" and consisting largely of sulfuric acid flows in the fibers’ interior. The sides of the fibers are studded with pores filled with a kerosene-like liquid, whose composition varies depending on the metal extracted. This liquid acts like a membrane, allowing the metal ions to migrate through the pores while the water remains outside. As a result, the metal concentration in the strip is successively increased. "Even though this concentration is eventually a thousand times higher than in the wastewater, the metals remain in solution due to low pH values," says Walachowicz. The extracted metals can be reused for electroplating.
A pilot plant has already been set up in Berlin that can purify 50 liters of wastewater per hour – which is not enough for full-scale commercial electroplating facilities. "But it wouldn’t be a problem in terms of technology to enlarge the plant," says Walachowicz. The CT pilot plant can treat one cubic meter of wastewaster for about 80 €. In contrast, it costs electroplating plants about 100 € to do the same with conventional—but not very environmentally compatible—treatment methods. And that doesn’t include the cost of disposing of the electroplating slurry.
Walachowicz and his colleagues are still developing a fully automatic control system for the plant. It will use a real-time analysis chip developed by a Siemens Corporate Technology team headed Dr. Frank Arndt. The chip features microscopically small channels. The metal content of tiny wastewater droplets can be analyzed directly on the chip on the basis of electrical conductivity. "From dosing and identification to the separation of metal ions—everything will take place on the chip itself," says Arndt. "What’s more, it will all be done electrically, without requiring any pumps or other mechanical aids." Arndt and Walachowicz plan to integrate the chip into the pilot plant later this year to allow automatic control of the system.
Ute Kehse