Intelligent Networking – RFID Applications
Taking Stock
Siemens is leading the way in development of radio frequency identification solutions (RFID). Now, major customers are starting to implement this new technology on a large scale. Initial applications in the field of logistics have been extremely promising.
RFID tags make the movement of goods faster and more reliable. For goods with a high water content, which could interfere with radio signals, flag tags are used. The transponder on a flag tag stands up from the package surface like a small banner
IThe big food warehouse is humming like a beehive. Bright-red forklifts whir as they move back and forth. They transport pallets of food cartons and lift goods up to shelves that can be as high as 18 m. The Rewe GmbH warehouse in Norderstedt, Germany, can accommodate about 30,000 pallets. About 3,500 pallets containing 1,600 different products, from canned goods and pasta to table wine, are brought every day to the distribution center on the outskirts of Hamburg. From here, they are transported to supermarkets all over northern Germany. Every day, warehouse workers load approximately 100,000 cartons from the pallets on to hundreds of small rolling containers that are then loaded onto trucks for the next stage of their journey. Of course, Rewe has an electronic goods monitoring system that supervises the complex movements of the pallets. But so far, the goods have been accompanied by delivery notes made of paper. That’s about to change. With the help of experts from Siemens Business Services (SBS) and other companies, Rewe is planning to switch to a paperless goods movement system. The new system will be made possible by RFID (Radio Frequency Identification) transponders, also known as RFID labels or tags. The tags contain a tiny chip and an antenna. In contrast to traditional bar codes, the chip can store more individual pieces of information, such as the item’s destination, its "best by" date and the producer’s address. A reading device can call up this information from a distance of approximately one meter using a weak radio pulse.
"Previously, a warehouse worker had to check every individual pallet and confirm its arrival within the system," says Meik Hunold, deputy director of the RFID project at Rewe. The use of RFID tags will considerably speed up this process in the future. Checking will then be even faster than it was with bar codes, because in order to register a bar code a warehouse worker has to read every individual code label with a hand scanner. By contrast, when truck drivers unload their vehicles the pallets provided with transponders are simply rolled into the warehouse through an RFID gate that registers the RFID information automatically. "A green light indicates that the palette has been correctly read," explains Hunold. After the truck has been unloaded, a glance at the monitor will reveal whether the delivery is complete. Missing pallets show up in red.
In the future, paper delivery notes won’t be necessary, says Hunold. At the supplier company, the dispatch of goods is registered via RFID and an electronic confirmation is sent to the warehouse. When the goods arrive in Norderstedt, the RFID system automatically registers the pallets. Within seconds, the central computer then compares the order with the goods actually delivered. "Another advantage is that we can monitor the goods without interruption," Hunold adds. The system automatically registers when goods leave the factory or the forwarding agent. Today, 30 of the company’s approximately 300 suppliers are linked with the RFID system. In coming months, the goods dispatch area and even the shelves and forklifts will be equipped with transponders. That will enable the forklifts to automatically detect mistakes. If a driver is about to put a palette in the wrong place on the shelves, a warning signal will sound, thus avoiding time-wasting searches for misplaced goods.
At Rewe’s RFID lab, tests are conducted to find out how RFID tags perform in practical applications. The transponders (right) are glued under the paper labels of packages. The long strips are the antennas, and the black point in the middle is the microchip
Goods with Flying Banners. Although RFID transponders have been in use for a number of years for tasks such as marking vehicle bodies on automakers’ assembly lines (see "Logistics – Warehousing" in Pictures of the Future, Fall 2003, and "Transforming Production with Tiny Transponders" in Fall 2002), many practical questions still remain unanswered. For example, it’s well known that metal interferes with the transponders’ reading process. But for some time it was impossible to know beforehand whether a given palette of vacuum-packed coffee or jars of pickles would cause problems. Researchers at Nordersted solved this problem by testing 1,600 products for readability. In the process, they learned that products with high water content or packaging that was made of aluminum interfered with the radio signals. The RFID specialists solved the problem by gluing the transponder tags onto such products in such a way that one edge sticks up like a banner. These "flag tags" can be easily read.
Monitoring Valuable Products. In addition to Rewe, a number of other companies are working with Siemens on RFID applications. Otto Group, the world’s largest mail-order house, and the Hermes shipping company, for instance, launched a joint pilot project in this area in August 2004. "We wanted to test whether RFID technology was feasible in practice and whether it would enable us to monitor goods continuously," says Roland Nickerl, head of logistics systems development at Otto. The aim was to improve the monitoring of valuable goods in particular. SBS initially equipped some 20,000 digital cameras, mobile phones and notebooks with RFID tags and supplied readers for the goods dispatch area at Otto and five Hermes depots. As Nickerl explains, the advantages are obvious. "Unlike bar codes, tags can be read even when they’re scratched or dirty. Furthermore, they can also be used for bulk shipments." In other words, RFID makes it possible to read a whole carton full of tagged items without having to open it.
But for Otto, still another key feature of RFID was crucial. "For us, the most important thing was the precision of the reading process." The company wanted the RFID system to operate at least as reliably as the conventional bar code system. As it turned out, the RFID system registered the goods dispatch at Otto, the incoming and outgoing movements at Hermes, and the delivery to the customers with an accuracy of more than 99 percent. The companies were impressed, and for the past few months they have been using the system in their everyday business. Specialists in Hamburg are now evaluating the data they have acquired to find out, for example, where goods get lost. "In some cases," says Nickerl, "mistakes are made when the goods are packed or loaded, and some articles end up on the wrong shelf." Transponder technology is now creating the transparency that is needed for an analysis of transport channels. "We can achieve significant cost savings with RFID, but because of high associated operating costs we have to plan our application strategy carefully," says Nickerl. "At a cost of less than three euro cents per transponder, it would be worthwhile to put RFID tags on around half of our items."
About 40,000 individual items are currently equipped with transponders. Because of data protection laws, the tags contain only the packages’ article and identification numbers, but no personal customer data.
Another major obstacle to the mass use of transponders on one-way packages such as milk cartons, as opposed to bar codes, is the high price of the transponders. RFID tags made of silicon currently cost about 0.30 €. But a solution is within reach. In the future, cheap transponders will be printed by the thousands on foil, thanks to plastics that conduct electricity and can be processed in the same way as ink from a printer. One of the companies driving this technology is Erlangen-based PolyIC, a spin-off of Siemens Corporate Technology (see Pictures of the Future, Fall 2004, The Chip Printers).
Intelligent labels. At the LogMotionLab in Magdeburg, the Fraunhofer Institute and Siemens are testing smart labels—tags equipped with RFID transponders
Tracking Fake Medications. Unlike Otto Group, pharmaceutical firms clearly see their business operations threatened by criminal organizations. The sector estimates that today every tenth package of medicine contains a fake product. Some 70 % of the cases that come to light occur in developing countries. What’s more, experts estimate that pharmaceuticals valued at $40 billion disappear every year. In view of these figures, the U.S. Food and Drug Administration has prescribed that batch tracing be implemented by 2007—and has suggested the use of RFID technology. With this in mind, Swiss packaging manufacturer Limmatdruck/Zeiler is currently working with SBS to develop a solution in which transponders would be attached either to the outside packaging of medicines or, depending on the value of the products, on the packaging of individual products, ampules or syringes. That would permit the items to be marked in a foolproof manner. If the transponders were linked via the Global Positioning System, the whereabouts of the batch could even be tracked. In combination with temperature sensors, it may even be possible to find out whether sensitive medications have been continuously cooled during transport. Lawmakers are also calling for RFID technology to be used in the food industry to comprehensively document the origin of the foods we consume.
It’s clear that RFID is a hot topic. Nevertheless, many companies still do not realize the advantages this technology could offer them, according to Helmut Röben of the Fraunhofer Institute for Factory Operation and Automation in Magdeburg, Germany. Röben, who has a degree in commercial engineering, is in charge of a special RFID research facility, the LogMotionLab, which is operated in cooperation with Siemens. Here, visitors interested in RFID will find a huge selection of state-of-the-art transponders as well as read/write units.
A number of conveyor belts rattle through the middle of the lab’s light-flooded workshop. Here it’s possible to test how tags should be attached to products so that they can be read clearly, and what kind of transponders and readers are best suited to a particular task. After all, different types of tag work with different frequencies and have different ranges. The LogMotionLab also has a mobile laboratory that can be used to quickly construct RFID installations on customers’ premises for on-site testing—without spending a great deal of time and money. "Our most important task is to work together with our customers to develop ideas," says Röben. "After all, it should be possible to integrate RFID systems smoothly into ongoing operations so that the customer can improve profits, either by saving time or through more efficient data management."
Once a customer-specific solution has been developed, specialists from Siemens can implement it. "Siemens is one of the world’s leading suppliers of RFID solutions," says Markus Kehrwald, head of RFID operations at SBS. "We’re the only company that offers products and services for many sectors along the entire RFID value chain. For example, the Siemens subsidiary Dematic provides material flow solutions. Siemens Automation and Drives develops transponders and read/write units, and SBS provides consultation, integrates RFID into IT systems, and implements RFID projects."
Working with Intel and SAP. Siemens has been working with Intel in yet another laboratory—the RFID Technology Center in Feldkirchen near Munich—since March 2004. Among other projects, the specialists at the Center demonstrate the integration of RFID in product planning systems. Another cooperation partner is SAP, which is based in Walldorf, Germany. In Feldkirchen, RFID systems are developed and linked with software from SAP, for instance, for the automatic registration of product dispatches. In addition, automotive industry solutions—for example, for kanban processes—are shown.
In contrast to centralized production planning, in kanban processes the necessary materials, such as components from suppliers, are ordered as needed. If a Kanban container for a certain component is empty, an order form is attached to it and it is sent back to the supplier. By using RFID tags to replace conventional order forms, the process can be automated and made faster and more reliable. According to Robert Hülsebusch, head of Intel’s RFID Technology Center, in many cases an employee will collect the order forms and not enter the figures into the system until the evening. But if RFID tags were used, the empty containers could simply be placed near the reader, which would automatically reorder the components in question. "This illustrates that even advanced processes can be further optimized using RFID," says Hülsebusch. Intel is contributing its special hardware expertise to the project. "We foresee significant market demand for read/write unit components, and of course for server structures to process associated RFID data," says Hülsebusch. If researchers succeed in developing inexpensive components that are coordinated with one another and in processing their data flows efficiently, RFID technology could really take off in the near future.
Tim Schröder