Auto Electronics – Driver Assistance
Sensors See the Light
Human eyes are sometimes just not enough on today’s busy roads. Assistance systems can help reduce stress and improve safety by monitoring traffic conditions and warning drivers of potential dangers. Siemens VDO has developed pro.pilot, a system that unites a number of automotive assistance systems. The technology was showcased at this year’s International Motor Show in Frankfurt.
Advanced sensing systems enhance safety. A night-vision system can detect pedestrians (large image) better and sooner than full-beam headlights. Sensors for blind spots (bottom right), for automatic parking assistance (center), and for trafficsign recognition—and combinations of these (left)—provide drivers with crucial safety-related information
It’s a nightmare scenario for any driver. There you are, peacefully driving along a dark country road, and all of a sudden a pedestrian or a deer appears in the headlights, right in the middle of your path. With adrenaline pumping, you brake and swerve to avoid contact.
In today’s vehicles, systems such as ABS and ESP already help drivers deal with such situations. Moreover, with the advent of new and more powerful assistance systems, such situations might be prevented altogether. A night-vision system, for instance, can recognize an obstacle on the road long before it appears in the headlights, and warn the driver accordingly. Recently, in the context of the 2005 International Motor Show in Frankfurt, Siemens VDO Automotive presented a car featuring a total of ten ground-breaking assistance systems.
Sensors: Different ways of seeing
Such systems enhance the driver’s view, prevent the car from wandering from one lane to another, and maintain a constant distance from the next vehicle. The one thing they don’t do, however, is to relieve the driver of responsibility for controlling the vehicle.
"Even in ten or twenty years, assistance systems will still be there to support drivers—but not to replace them. The driver will always have the final say," says Dirk Zittlau, head of Driving Assistance Systems at Siemens VDO Automotive in Regensburg. Zittlau, an electrical engineer, also rejects the fear that these technologies could somehow take control of vehicles. "The driver will always be able to overrule such systems. Besides, it will probably be possible to deactivate some of them as well, if drivers feel distracted."
Cutting Fatalities by 50 %. Behind the push for advanced driver assistance systems is the stated goal of the European Union to halve the number of road fatalities by 2010, based on the 2001 figure of around 40,000. Experts agree that this is barely feasible without the use of electronic assistance systems. Indeed, experience with the Electronic Stability Program (ESP) already confirms this. According to a study by the U.S. National Highway Traffic Safety Administration (NHTSA) covering the period between 1997 and 2002, the number of single-vehicle accidents—i.e. accidents that don’t involve another road user—and fatalities involving large SUVs equipped with ESP have both fallen by two thirds. Similarly, the number of single-vehicle accidents involving passenger cars with ESP has fallen on average by 35 % in the U.S.
What Consumers Want. Demand for driver assistance systems is also coming from consumers themselves, primarily because the average age continues to edge upward (see Pictures of the Future, Spring 2005, The Graying Society: When I´m 64). "In the future, more and more older people will want to keep driving, despite increasing physical impairments and slowing reactions. Here, our lane-change assistant—to name just one example—can help to compensate for a driver’s limited mobility and restricted vision," says Zittlau. Using radar sensors to monitor traffic to the right and left of a car, this system warns the driver of any objects that pose a danger should he or she wish to change lanes or execute a right or left turn. In addition, before the doors are opened to leave the vehicle, the same sensors also warn of approaching cyclists, skaters or cars concealed in the mirror’s blind spot.
Follow that car! – New driver assistance systems from Siemens´ labs
It’s stop-and-go time on the highway again, and all that braking and accelerating is really stressing drivers out. To help prevent rear-end collisions in congested traffic, Siemens is developing a system that can maintain a constant distance from the vehicle in front, automatically braking and accelerating the car as required. What’s more, the system can even do this when driving around corners, as demonstrated by a test vehicle at the end of April 2005 in the "Invent" project sponsored by the German Ministry of Education and Research to promote user-friendly technology for intelligent transportation. The car is fitted with a video camera and an infrared laser (lidar), mounted on the windshield, plus radar sensors fitted behind the front fender. "The various sensor systems and the areas they scan all complement one another," explains Dr. Georg von Wichert from the Competence Center for Autonomous Systems at Siemens Corporate Technology. As Wichert explains, this mix of different sensors increases the power and reliability of the system as a whole: "After all, there’ll always be times when individual sensors are impaired by ambient conditions." The image-processing system hooked up to the video camera is able to calculate—on the basis of their distance ahead—whether vehicles in front are accelerating or decelerating. In addition, the system also registers road markings—which serves to determine, among other things, lane width and curvature. Using this information, a motor fitted to the steering column of the test vehicle is able to hold it automatically in the middle of the lane and even follow the car in front as it drives around a corner. In combination with a lidar sensor, a radar system measures the distance to, and the speed of, vehicles in front. Unlike today’s systems such as automatic cruise control (ACC), which work best at high speeds and are unable to steer the vehicle, this new system can control the car fully automatically at low speeds of between zero and 50 km/h. This is made possible by special software that checks the data from all three sensors—video, radar and lidar—millisecond intervals in order to verify that their readings do not contradict a model of the vehicle environment. The latter features descriptions of probable vehicle movements, as based on the laws of nature. If, for example, the sensors have registered a vehicle in front that is driving at a certain speed, the model tells the system that the vehicle will probably continue to travel at that speed. Because the system knows its own speed, it can calculate where the vehicle in front should be by the time of the next reading, which in turn is compared with the new sensor data. In this way, the system can determine the precise position of the vehicle in front and therefore ensure that it remains at a safe distance. Of course, the driver can also overrule the system at any time and independently accelerate or brake the vehicle.
Rolf Sterbak
Another factor spurring growth in this field is the growing need for enhanced driving comfort. Anyone who has ever spent a long period in congested highway traffic knows the stress of having to switch constantly between the gas and brake pedals. “That’s cally focuses on the next vehicle ahead and resets the optimum distance and speed.
The Lane Departure Warning (LDW) system functions according to the same principle. Here, a video camera monitors lane markings. If the software detects that the vehicle is in danger of crossing the white line, it produces a clearly discernible vibration in the automatisteering wheel so as to warn the driver. In the future, the LDW could also be transformed into a camera-controlled lane-guidance system, which would automatically correct the steering whenever the vehicle threatens to stray off course.
Virtual road signs. In the future, important traffic information could be projected on the windshield
In another highly useful development, Siemens VDO has come up with software that can read speed limits on traffic signs. If the driver violates a speed limit, the system displays a visual warning signal. "But it won’t automatically reduce your speed," Lutz emphasizes. "Furthermore, the driver can always deactivate the system," he adds. In addition, there are now plans to extend the system to cover stop and yield signs. Meanwhile, another application from Siemens VDO—adjustable cruise control (ACC) featuring variable speeds—utilizes a new light-based detection technology to measure distance. This so-called lidar sensor is comparable to conventional radar sensors, but is substantially cheaper. Moreover, unlike radar sensors, which have to be fitted behind the radiator grille or the fender in order to protect them from the elements, lidars can simply be installed behind the windshield.
Robots that can recognize locations
Researchers at Siemens Corporate Technology in Munich are busy looking at how machines can develop a sense of direction in unfamiliar surroundings. For some time now, Michael Fiegert and his team from the Competence Center for Intelligent Autonomous Systems have been working on self-propelled robots for applications such as transport systems in hospitals and cleaning equipment in supermarkets and warehouses. "The same principles can be applied to other moving objects that utilize visual-recognition systems. In the future, this might include cars equipped with cameras," says Fiegert. At present, Fiegert’s team is using laser scanners to generate 3D images of a robot’s immediate surroundings. In the future, however, these will be replaced by cheaper video cameras. The principle is the same. Images of certain places are taken from different perspectives and at varying resolutions. On this basis, characteristic features are determined and then saved in the form of a code. The same characteristic features are then coded from another angle in order to calculate their 3D positions in the space under consideration. Using this method, a mobile machine is able to work out its position in relation to its environment. Whenever it returns to a given location, the machine recognizes it on the basis of the characteristic features saved in its memory. Siemens has recently installed this technology in a driverless forklift designed to independently transport pallets around a warehouse. The project is already so advanced that Fiegert is confident that the system will be used in practice in the near future.
Rolf Sterbak
Even at night, Siemens VDO helps keep drivers fully in the picture with two night-vision systems, one short-range and one longrange. The short-range system emits infrared light—which is invisible to humans—at a wavelength of around 900 nm. Any reflected infrared is then picked up by a special video camera mounted near the rearview mirror. On this basis, the system then generates a realistic black-and-white image of the road ahead to a distance of 150 m, which is shown on either a monitor or a head-up display on the windshield. The second night-vision system features a thermal-imaging camera, which registers the temperature difference of objects in comparison to their environment at a range of up to several hundred meters.
Synergistic Networking. Combining various systems—a major Siemens VDO strength—brings extra benefits. If a car’s navigation system recommends leaving the highway, LDW will then monitor whether this maneuver can be carried out safely. And should the driver be unable to change lanes in time, the navigation system will have already calculated an alternative route before the turn-off point, so as to spare the driver needless stress. In another example, a so-called electronic horizon prevents a similar scenario. As your car turns off the highway on to the exit road, it’s conceivable that the adjustable cruise-control system could lose the vehicle ahead and then accelerate to the preset speed. However, using digital maps and a GPS device, the system recognizes that your car is on the exit road and adjusts the cruise control accordingly. Networking also brings benefits in other areas, not least when different applications utilize the same sensors. For example, the small CMOS camera is utilized by the system to read road signs, the LDW system, the stop-and-go assistant and—albeit with a different lens—the night-vision systems.
Augumented Reality enhances navigation systems
Navigation systems featuring augmented reality could soon be providing drivers with enhanced assistance. With this system, the driver’s actual view of the road ahead is supplemented by virtual, computer-generated information. "We’re currently working on a prototype that may well develop into a product in a few years," says Dieter Kolb, a software engineer at Siemens Corporate Technology. Today’s systems present route information as a pixilated graphic or a map representation on the display unit, accompanied by voice output. In the future, however, the route could be displayed as a colored strip superimposed on images of the road ahead, as captured by an onboard camera. The driver would then see the route as if it were literally painted on the road. And because the display would show the same view of the road ahead that the driver sees through the windshield, motorists would have no trouble orienting themselves. Moreover, the "pathfinder" provides clear routing information at night or when the driver’s view of the road ahead is obscured by other vehicles. For example, the system shows the driver the course of the road after a hill or a tunnel and therefore gives advance warning of any sharp bends or other potential trouble spots. In the next project stage, route information will be projected directly onto the windshield—although only when required, so as to guarantee a free view of the road at all other times. If navigation assistance is needed, the driver simply presses a button on the steering wheel in order to project routing information onto the head-up display on the windshield. A major advantage of augmented reality is that the driver always keeps an eye on the road ahead even when consulting navigation data. In other words, this solution will not only improve the ergonomic characteristics of today’s navigation systems but also increase road safety.
Rolf Sterbak
Less Can Mean More. Natural human limitations make it impossible to operate and read different assistance systems at the same time. "The important thing is to ensure that new systems and the readings they produce are integrated in a sensible way," suggests Prof. Henning Wallentowitz, head of the Institute of Motoring at Aachen Technical University, Germany. "Ultimately, the quality of the man-machine interface will be the determining factor in deciding whether drivers will be willing to accept future assistance systems," he says.
Siemens VDO has therefore produced a comprehensive concept to ensure maximum user-friendliness and minimum strain on drivers. This includes siting display devices in locations where drivers intuitively expect to find them—a TFT display in the instrument cluster, for example, or a larger screen in the center console and warning lights where they can best be seen. The centerpiece here is the fully configurable head-up display, which projects driving-related information straight onto the windshield, directly in the driver’s field of vision. Siemens VDO is currently the only company to supply such a system, which has featured in the BMW 5 series since 2003.
Some of today’s upper-range vehicles already feature special gas sensors that sniff the air for noxious exhaust fumes. If necessary, the air conditioning will then switch temporarily to circulation mode or even feed the air through an activated carbon filter so as to remove carbon monoxide and nitrogen oxides. "Our goal is also to filter out other unpleasant smells—such as those from smog or road resurfacing work—from the air inside the car," says Dr. Maximilian Fleischer from Siemens Corporate Technology. Fleischer is currently working on new odor sensors (photo). In the past, researchers had to build a separate sensor for each gas. Now, however, they are developing a silicon chip that combines a number of sensors and can thus detect around five gases. Each gas is identified by means of a special chemical coating around one square millimeter in size. Choosing the right materials for these coatings requires considerable expertise. Certain metal oxides, for example, are used to detect pollutants from exhaust emissions (see Pictures of the Future, Fall 2004, Gas Sensors: Digital Bloodhounds). A further challenge for researchers is to design these coatings so that they only retain the gas molecule long enough for the gas to be identified and then release it so as to free up the sensor for further tests. Gas molecules are identified on the basis of the electrical pulse they generate when in contact with the coating. Fleischer’s team is also working on so-called feel-good sensors that measure the humidity, temperature and carbon dioxide content of the air inside the vehicle. If carbon dioxide content rises above 1,000 ppm (parts per million), the driver will start to tire. In a full car with no ventilation, this level is attained within 15 minutes or so. "Our goal is that vehicle occupants should feel absolutely at home in their cars," says Fleischer. Given that activated carbon filters can only absorb a limited amount of malodorous substances, researchers are looking at other types of filtering techniques. These include odor-busting substances such as complex dyes, which can be applied to the roof liner, for example. When these dyes are stimulated by light, they temporarily bind and activate oxygen molecules from the air and can thus decompose odor molecules through a process of oxidation.
Rolf Sterbak
A sophisticated control system regulates which information is displayed where and in what kind of driving situation. This, according to Wallentowitz, is essential if the technology is to be user-friendly. Information is distributed on the basis of both ergonomic findings and usability tests with typical drivers. In general, the information with the highest priority is shown in the head-up display, while less important data appears in the instrument cluster or on the screen in the center console. The system also presents information in locations most convenient for the driver. For example, the warning light for the LDW system is mounted in the door panel, near the side mirror.
Jürgen Goroncy