Go to content

SIEMENS

Research & Development
Technology Press and Innovation Communications

Dr. Ulrich Eberl
Herr Dr. Ulrich Eberl
  • Wittelsbacherplatz 2
  • 80333 Munich
  • Germany
Dr. Ulrich Eberl
Herr Florian Martini
  • Wittelsbacherplatz 2
  • 80333 Munich
  • Germany
pictures video

An energy automation system known as "SoEasy" works with Personal Energy Agents (PEAs). The agents automatically broker power capacity and prices.

An energy automation system known as "SoEasy" works with Personal Energy Agents (PEAs). The agents automatically broker power capacity and prices.

Simulation of a section of a smart grid in Siegen, Germany.

Simulation of a section of a smart grid in Siegen, Germany.

How to Simulate a Smart Grid

Substantial research is still required in order to develop technologies for tomorrow's smart grids. Engineers from Siemens Corporate Technology are devising the software needed to incorporate diversified and distributed power generators into the electricity network.

Image Personal Energy Agents broker generated power.

How will tomorrow’s grids handle fluctuating energy from vast numbers of solar and wind-based electricity producers? The honest answer is that no one know. Major questions include pricing uncertainties and increasing variability of supply and demand. Yet help could be at hand in the form of software developed by Christian Glomb from Siemens Corporate Technology (CT). Glomb’s software simulates a smart grid in its capacity both as a network for transmitting electricity and as a communications network. The project is Siemens’ contribution to “Software Platform Embedded Systems 2020” (SPES), a program funded by the Federal Ministry of Education and Research in which Siemens simulates a hypothetical smart grid in Siegen, Germany. SPES’s goal is to develop processes for the embedded systems market, i.e. control software that is installed in equipment and manages transport systems and power grids.

The software builds on a conventional power grid simulation and enriches it with a realistic emulation of communication between various system components and a simulation of control functions for the system as a whole. It comprises all the major elements and processes that are required for proper and stable functioning of the grid. Given, for example, that communications networks can be susceptible to problems, it is important to make this aspect of the system as robust as possible.

Using data regarding transmission and communication networks, power generating plants, and consumers, the software calculates the probable behavior of system components. On a sunny Sunday, for example, when lots of power is produced by photovoltaic plants but little is consumed by industry, the software can recognize when maximum voltages are exceeded and a tap transformer is required to deal with the surge. “The software tells us how the system will behave before it even goes into operation,” says Glomb.
The simulation does not extend down to the level of individual appliances, even though this would be feasible. Instead, it assumes an overall load profile for the connection points of households or commercial enterprises. Otherwise the complexity of the control functions would become unmanageable. It took a year for Glomb to program the basic simulation, followed by a couple of weeks to model a concrete grid. Initially, Glomb and his Siemens colleagues in Vienna modeled a smart grid in Eberstalzell, Austria, which is scheduled to go on line in 2013. This grid will comprise between 150 and 200 connection points, as many as 70 photovoltaic plants, and about the same number of electric vehicles. The simulation is, however, constructed in such a way that it would also be possible to create much larger grids that comprise several thousand connection points.

When it comes to smart grid technology, the future has already arrived in Wildpoldsried. Using photovoltaic, wind, and biomass generation, this picturesque town in southern Germany produces over three times the power required to cover its own demand. In a project named IRENE , local utility Allgäuer Überlandwerke (AÜW) and Siemens are investigating how smart grids can cope with a massive infeed of renewable energy. According to Michael Fiedeldey, Head of Technology at AÜW, power grids need to become more intelligent in order to smooth the transition to a new energy age. He calls for “smart technology rather than more copper.” That will not only spare the expense of installing new transmission lines but also create new services and new value-added chains for his company.
At the heart of the field test is a smart software system developed by Siemens. This energy automation system, named SoEasy, creates a virtual market that enables operators of biogas-fired and photovoltaic power plants to sell their product to a central purchaser — in this case, AÜW. In the case of IRENE, the main focus is on the integration of distributed power plants and electric vehicles. Here, the system optimizes the management of energy storage facilities — for electricity, heat, and gas — connected to the grid, with the aim of avoiding peaks or overloads.

SoEasy functions by means of software agents that automatically broker power capacity and prices. The following agents exist:
Personal Energy Agent (PEA): Every facility in the smart grid, whether a power producer or consumer, is equipped with this small device. It contains a computer with interfaces to the facility and to the Internet. Using a PC, plant operators can stipulate how much power the owners want to sell, at what time, and at what minimum price. Every 15 minutes — other intervals can be set — the PEA brokers power capacity and prices with a Balance Master.
Balance Master: This software agent, installed at a utility, decides which PEA offers it will accept in order to cover demand in the grid. Details regarding the technical operation and pricing strategy of power plants connected to the PEAs are not provided to the Balance Master; this information remains in the hands of the plant operators. As a rule, planning is conducted for the coming 24 hours, though shorter periods to permit participation on the intraday market are also feasible.
Area Administrator: This agent helps the grid operator maintain network stability. The software only intervenes when maximum voltages are exceeded. For example, if too much solar power is being fed into the grid, the area administrator can either modify the infeed from other plants via commands to their PEAs, or adjust the ratio of a distribution transformer. This is now being done for the first time in Wildpoldsried.
Network Transport Agent (NTA): This agent collates data from plants, electricity meters, and the grid and displays it in visual form in the network operator’s control room. The NTA supplies this information to the Area Administrator, which decides whether intervention is necessary, and to the Balance Master, which decides which offers of power can be accepted without overloading the grid.
Energy Police: This agent ensures that all agreements are kept, that plant operators supply the power promised by their personal energy agents, and that no power is illegally siphoned off.

“The IRENE project’s software agents don’t deal with real money,” says CT engineer Dr. Michael Metzger, who played a big part in developing the system. “But SoEasy is technically capable of networking hundreds of thousands of power plants, so in the future it could be used for trading on real power markets.”
Working with colleagues from Siemens’ Smart Grid Division, Metzger is now busy turning the functions and components from field test into products and services for the Siemens portfolio. For example, elements of IRENE are already in use in other reference projects, including one on the Danish island of Bornholm. At the same time, IRENE profits from technology from other CT research programs. For instance, a similar project in the Harz region of Germany has provided modules to incorporate and automatically implement communication protocols.

In the Harz project, CT researchers are now testing a tiny box called a “power bridge,” which provides a communications interface between the grid and a whole variety of distributed, independent power generators and consumers. These include combined heat and power plants, fuel cells, and swimming pools. Power bridge is used wherever power plants feed electricity into the grid and also wherever energy storage facilities or power loads can be switched on to stabilize the network. These facilities automatically log on to the smart grid. “We looked at how the Internet service providers do it with their self-configuring DSL routers,” explains Jörg Heuer, Head of the Embedded Networks Research Group.
Power bridge has two interfaces: one to the power producer or consumer, and one to the public grid. Plant operators inform their specific power bridge whether they have extra capacity in either power generation or power demand. This data is then transferred to the control center in the form of a data model that is uniform for all plants. The control center then informs the respective power bridge how much extra capacity it wishes to accept. The power bridge receives no information as to how the plant operator actually meets this order. It knows neither the exact operational details, including any readings from the plant, nor how the operator calculates costs. Neither does it have any direct control over the plant. Instead, it serves as a gateway that guards the plant’s operational details and operating security against outside observation, but nonetheless provides the operator with a facility to market its current capacity.

Bernd Müller