Go to content

SIEMENS

Research & Development
Technology Press and Innovation Communications

Dr. Ulrich Eberl
Herr Dr. Ulrich Eberl
  • Wittelsbacherplatz 2
  • 80333 Munich
  • Germany
Dr. Ulrich Eberl
Herr Florian Martini
  • Wittelsbacherplatz 2
  • 80333 Munich
  • Germany
pictures

Plants handle water treatment at a Siemens facility in Kalwa, India, where 3,000 employees manufacture switchgear and transformers.

Plants handle water treatment at a Siemens facility in Kalwa, India, where 3,000 employees manufacture switchgear and transformers.

Plants handle water treatment at a Siemens facility in Kalwa, India, where 3,000 employees manufacture switchgear and transformers.

Backyard Sewage Plant

Water is a precious resource, especially in emerging markets. Siemens' facility in Kalwa, India, recycles its wastewater with one of the environmental initiatives that won the Vasundhara Award 2011 - a sewage treatment system that uses plants.

Image
Image Plants handle water treatment at a Siemens facility in Kalwa, India, where 3,000 employees manufacture switchgear and transformers.

Customized Water Recycling

Image open

Wastewater that requires treatment before it can be re-used differs widely. Not only can the water be clear or murky, it can also contain organic impurities, pathogens, or heavy metals. Siemens Water Technologies offers a wide range of customized products and solutions for removing harmful substances, while also achieving maximum energy savings. In addition to traditional methods, municipalities and industrial firms are increasingly demanding more compact and energy efficient technologies, such as the MemPulse Membrane Bioreactor (MBR) system from Siemens. The pores in the system’s membranes are so tiny that only water molecules can get through. Biomass, bacteria, and even viruses are prevented from passing through the pores. The system utilizes bursts of air along the membrane pores to prevent them from becoming clogged. Compared to conventional reactors, which continuously blow air through membranes, the Siemens approach reduces electricity consumption by more than one third. The EcoRight MBR system, currently under development, is designed to meet very stringent wastewater discharge requirements for wastewater re-use. Effluent from the MBR is fed to a reverse osmosis system, purifying the water further so it can be reused as boiler feed water, cooling water, and other process water. The EcoRight system has been successfully tested at one of the refineries of the world’s largest oil producer, Saudi Aramco, where it is treating wastewater from an oil/water separator. Quality standards for recycled water can also differ greatly. While some industrial plants re-use the water as cooling water or boiler feed, others use it for utility or process water. Additional treatment, if required for applications such as beverage or semiconductor manufacturing, is provided by advanced carbon filters, ion-exchange, distillation, electrochemical systems, and chlorination and ultraviolet disinfection systems. Another new development is Siemens’ Micro Media Column (MMC), which can remove heavy metals such as mercury and copper from water. In this filter, contaminated water flows down a column full of micrometer-size particles that chemically bind heavy metals. The water is purified at a throughput rate that is unmatched in the industry, with an effectiveness beyond the levels of today’s environmental requirements. Applications for the Micro Media Column include waste water polishing in power generation and ultrapure water polishing in the oil and gas industry. Andrea Hoferichter

close

Anyone paying a visit to the new sewage treatment plant at the Kalwa factory near Mumbai will think they have entered an oasis. Between production halls and areas covered with asphalt lies a small collection tank containing treated water — sparkling, turquoise-colored and clear as glass. Next to it is a gravel-filled basin in which meter-high reeds grow along with plants bearing red blossoms. “On an area of about 1,000 square meters, we recycle all of the wastewater from our four subplants, as well as from the administrative building,” says Jeevan Rao, who heads the Safety and Environmental department for Siemens Cluster South Asia. The new sewage treatment plant with its artificial wetland is an important part of Siemens’ environmental initiative, which was honored with the prestigious Vasundhara Award 2011 in June. The Vasundhara Award is the most important environmental prize of the southern Indian state of Maharashtra.

The water recycling system used at the Kalwa factory functions like a swamp. Instead of relying on advanced technology, the system employs an ecosystem of plants and microorganisms that eliminate harmful substances from the wastewater. The system features a cascade of 32 basins that treat the water mechanically as well as biologically. For example, the gravel holds back particles suspended in the water, while the plants produce oxygen and their roots ensure that the gravel bed is well ventilated. Bacteria break down organic substances — such as scraps of food or dirt from hand washing — into carbon dioxide and water. And nitrogen compounds such as proteins or urea are ultimately converted into harmless nitrogen gas. At the end of the cleaning facility, which is more than 90 meters long, the treated water is so clean that even mosquitoes aren’t interested in it any longer. A system of pipes then channels the water to the Siemens administrative building, and to the garden facilities and rest rooms, where the cycle begins anew.

Natural Advantages. “Besides being effective, inexpensive, and simple to maintain, the facility just looks idyllic,” says Rajiv Agaskar, Sustainability Officer for Siemens Real Estate India. “It enables us to save up to 12 million liters of water per year.” In addition, natural water recycling reduces the facility’s fresh water costs by up to €4,500 annually. What’s more, according to Agaskar, the facility cost less to build than a high-tech counterpart. The only technology the system needs is pumps and flow-rate meters, and it doesn’t have to be continuously monitored, as is the case with conventional sewage treatment plants.

Given all these advantages, it’s no surprise that sewage treatment plants equipped with artificial wetlands are becoming more popular worldwide. Their only drawback is that they take up a lot of space. A city of 100,000 inhabitants would need a facility almost as big as 60 soccer fields. And the facility has no control system, making it unsuitable for wastewater whose composition fluctuates greatly.

The newly constructed wetland in Kalwa recycles two types of wastewater, which are first separately collected and pre-treated. Most of this water comes from toilets, sinks, and the canteen. It is channeled into a precipitation tank, where solid substances that are sometimes very smelly can settle. The wastewater from the Siemens production halls primarily contains finely distributed oil droplets, which are pretreated separately before the water is sent to the wetland.

“All of the pre-cleaned water then flows through the wetland,” says Agaskar. The facility’s concrete basins in varied sizes are more than one meter deep and have a downward slope. Barriers cause the water to flow into a basin at the top and flow out again at the bottom. “Our facility purifies the water horizontally and vertically, achieving 95 percent efficiency — better than the 90 percent efficiency achieved by many conventional treatment plants,” Agaskar says.

Although India is home to 16 percent of the world’s population, the country has only four percent of the planet’s water reserves. “Groundwater levels are dropping by four centimeters every year,” says Agaskar. Climate change will probably make this even worse. Artificial wetlands alone will not be able to solve the problem. But as Agaskar and Rao say, “Every component is important.”

Andrea Hoferichter