Prof. Hans Müller-Steinhagen(55) has headed the Institute of Technical Thermodynamics at the German Aerospace Center (DLR) since 2000. After earning a PhD in process technology, he worked for seven years at the University of Auckland in New Zealand, before becoming a dean at the University of Surrey, UK. Working closely with designers and facility operators, Müller-Steinhagen’s teams have made solar electricity generation much more efficient. Their institute is today a global leader in its field
- Text Size
- Share
- Print this page
When will solar-thermal electricity become competitive?
Müller-Steinhagen: That depends on prices for conventional fuels — and in 2008, we saw just how volatile they can be. It also depends on the development of investment and operating costs for solar-thermal facilities. We’ve already overcome the first major challenge with the launch of the Desertec Industrial Initiative. As we begin producing more solar-thermal electricity, it will become cheaper. Costs will decline when large companies start using and further developing the technology. One result will be the mass production of components. I’m confident that we can become competitive in about 15 years.
Saving the world with big projects is a concept that has sometimes caused major problems — for instance in dam construction projects. Isn’t it possible that this could happen with Desertec?
Müller-Steinhagen: Although Desertec is a gigantic project as a whole, it’s also the sum of many smaller and more easily manageable projects. After all, many plants, each with a capacity of at least 50 MW, could gradually go online. That sort of value is common in Spain today. This approach will work because investment costs can be kept at a manageable level. And with the right financial incentives, such plants can be operated profitably. At the same time, the infrastructure needed to transport some of the energy produced in Africa and the Middle East to Europe involves projects that can only be successfully implemented by a large number of big companies — companies that can supply high voltage direct current technology and that also possess the necessary project expertise. Siemens is in a very good position to play such a role.
What type of research still needs to be performed?
Müller-Steinhagen: Our main goal is to increase electricity production efficiency. If we could increase our efficiency to 20 % from the current average of 15 %, we could reduce the area needed for the mirrors by one-third. Don’t forget that the collectors account for nearly half of the total investment cost. We’re also experimenting with direct steam generation, where water in the receiver tubes is converted into steam and sent on directly to the turbine. We have worked with Siemens here on liquid separators. Losses can also be minimized through the use of different storage media. So, if we can boost efficiency through many measures, even if it’s just one percentage point at a time, the cumulative effect over the lifespan of a facility could be substantial. The German Aerospace Center is therefore working closely with Siemens in many areas to ensure that the solar-thermal plants of the future will be built in the near, rather than in the distant, future.
Three Ways to Put Solar Power to Work
open