Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Welcome

Partnering for a Sustainable Energy Future

Please join Siemens at POWER-GEN International 2016 Exhibition and Conference in Orlando, FL! With a comprehensive portfolio that spans the energy spectrum, we are helping our customers generate electricity in an economically and environmentally sustainable way.

Innovation drives sustainable energy. Siemens is the market leader in digitalization and sustainable energy creating real value by enabling our customers to make smarter choices.  New product innovations and new technologies coupled with global energy market expertise enables Siemens to deliver efficient, reliable, and flexible power generation solutions and services across the entire energy system.

We provide in-depth expertise to enable our customers to master the challenges associated with fossil-fuel-based power generation, oil and gas, intelligent power networks, energy storage and energy efficiency.

Siemens offers the industry's most comprehensive industrial and aero-derivative gas turbines, steam turbines and compressors portfolio. This gives our customers more choices from a single provider.

Join our Siemens experts at Booth 5100 and learn how we can help you meet your individual business needs.

Highlights

Our highlights

Willi Meixner, CEO of the Siemens Power & Gas Division

The Power to Change – Opening Keynote Session

While there are many trends shaping and re-shaping the energy landscape, Willi Meixner, CEO of the Siemens Power & Gas Division, will focus on a vital few that are likely to have the largest impact in the coming decade:  Distributed Energy, Digitalization and Cyber Security, and Storage Technologies. He will provide an up close perspective on these trends and the main challenges associated with them, focusing on the key question about how these trends potentially threaten the traditional business models that have been part of our industry for decades. Meixner will also address how these developments impact existing challenges being addressed by governments and policy makers, such as CO2 reduction and an affordable energy supply. Finally, he will share his thoughts on how we, as an industry, must tackle the upcoming evolution together. 

When
: Tuesday December 13, 9:30 am – 11:30 am
Where: Exhibit Hall NA1, North/South Building

image

Virtual reality at our booth

Visit us and enjoy an interactive Virtual Reality experience. This realistic simulation of our gas turbine SGT-800 is something you won’t want to miss! 

image

Generator swichgear

HB3 is the first generator switchgear worldwide with vacuum generator circuit-breakers for ratings up to 12,500 A with natural cooling and a switching capacity of 100 kA type-tested according to the IEEE C37.013 standard. It offers maximum operational reliability and a high degree of personal safety, as short circuits between phases are excluded due to the single-phase encapsulation. As a result of the flexibility of the phase spacing and diameters of the single-phase encapsulated IPBs, the HB3 fulfills all requirements for integration into the generator leads. The switchgear can be operated with the overpressure needed for the IPB system. The switchgear is type-tested in accordance with the standards IEC 62271-200 and IEEE/IEC 62271-37-013. The HB3 generator switchgear is suitable for power plants up to 400 MW depending on the type of power plant and the operating voltage.
More information

image

Innovating Electrical Generators with Siemens State-of-the-Art Pressurized Air-Cooled technology

Siemens SGen-2000P series pressurized air-cooled generators with ratings up to 550 MVA are used in gas turbine and steam power plants. The SGen-2000P series features pressurized-air cooling with a water-cooled stator winding. Replacing hydrogen cooling with pressurized air significantly reduces plant complexity and operational cost. 

To learn more please visit our presentation on Tuesday, December 13, 2016, 1.30-3:30p.m.

More information

Agenda

Conference

Hear the Siemens speakers during the conference

13:30 – 15:30 | Panel Discussion: Latest Combined Cycle Designs – Flexibility and LowerInstalled Costs

Panel Discussion: Latest Combined Cycle Designs – Flexibility and LowerInstalled Costs

Mat Palmer

 

Download Agenda (PDF)

Advancements in O&M Practices and PerformanceImprovements

Application of GT Upgrades for the SGT6-5000F (W501F) Gas Turbine

 

Harvey Stinnett

 

Download Agenda (PDF)

Innovative Trends in Power Plant Operations

Innovating Electrical Generators with Siemens State-of-the-Art Pressurized Air-Cooled technology

 

James Zborovsky

 

Download Agenda (PDF)

Improvement in Boiler Operation and Performance

Improving Performance and Achieving Heat Rate Reductions in Fossil Units to Meet Clean Air Act Guidelines

 

Michael Smiarowski

 

Download Agenda (PDF)

From Smart Monitoring & Diagnostics to Prediction: Data Analytics and the Plant of Tomorrow

Leveraging Digital Services to Maximize Customer Profitability

 

Karen Ratclif

 

Download Agenda (PDF)

09:30 – 11:30 | Applications in Combined Cycle I

Applications in Combined Cycle I

HRSG Construction Options for Achieving the Lowest Installation Cost in Combined Cycle Power Plants

 

Patrick Albert

 

Download Agenda (PDF)

Small and Medium Gas Turbines

Flexible Power Generation for Grid Support Utilizing Aero-derivative Gas Turbine Technology

 

Michael Welch

 

Download Agenda (PDF)

Financing Projects in Domestic Capacity MarketsPanel Discussion

John O’Brien

 

Download Agenda (PDF)

GT Performance and Techno-Economic Improvements

Application of GT Upgrades for the SGT6-5000F(3) (W501FD3) Gas Turbines

 

Michael Salvatore

 

Download Agenda (PDF)

Making CHP Work for You

CHP: Maximizing Energy Efficiency, Minimizing Environmental Impact and Reducing Operational Costs

 

Dalia El Tawy

 

Download Agenda (PDF)

Applications in Combined Cycle II

Expanding Options for Combined Cycles

 

Bonnie Marini

 

Download Agenda (PDF)

Gas Turbine Component Advancements

GT-ACO: Gas Turbine Autonomous Control Optimizer

 

Ashtad Kotwa

 

Download Agenda (PDF)

Reliability & Optimization of Steam Turbines

Life Extension and Efficiency Improvement: Ghazlan Power Plant Units 1-4 Steam Turbine Upgrade Project

 

Joseph Bullock

 

Download Agenda (PDF)

10:00 - 11:30 | Panel Discussion: The Digital Power Plant is Disrupting Traditional Power Generation. What is It and Where is It Going?

Panel Discussion: The Digital Power Plant is Disrupting Traditional Power Generation. What is It and Where is It Going?

Aymeric Sarrazin

 

Download Agenda (PDF)

Panel Discussion: Large Frame Gas Turbines

Joshua Kovac

 

Download Agenda (PDF)

Our Products

All from a single provider

Get a first glimpse of our booth