Jens Hald Jensen believes the time has come to create a new energy system. Why? Because he’s convinced that the transition to a sustainable energy infrastructure can stop climate change. And because he wants to pass on to future generations a world worth living in. Jensen, a Siemens employee who’s project manager at the test center for wind turbines in the Danish town of Østerild, is working every day to make our energy supply a little bit greener – one step at a time.
Making a successful transition to a new energy system will require implementing a complex puzzle of measures. As an integrated technology company, we offer a virtually unrivaled portfolio of products and solutions spanning the entire Power Matrix. On the following pages, Jens Hald Jensen describes how he’s taking personal responsibility to help shape the future of energy. And in an interview with Dr. Hans-Josef Zimmer, Chief Technology Officer for our key customer EnBW Energie Baden-Württemberg AG, you’ll learn how one of Germany’s major utility companies views that future.
ABOVE – Clear instructions for the team: Siemens engineer Jens Hald Jensen (left) oversees the assembly of the wind turbine with the longest rotor blade currently in operation worldwide.
LEFT – A logistical tour de force was required just to transport the Siemens B75 rotor blades 320 kilometers from the Danish port of Esbjerg to Østerild.
“At 75 meters in length, the new rotor blades have nearly the wingspan of an Airbus A380.” When Jens Hald Jensen talks about his work, he makes generous use of superlatives. And today is a very fitting occasion for them: on this gorgeous August day, the Siemens engineer is supervising the assembly of the world’s largest wind turbine rotor. Sporting a white hardhat and neon-yellow safety vest, Jensen stands in the middle of a test center in the Danish town of Østerild, where we’re testing our latest products before they are commissioned on site. The test subjects arrived several days ago: our SWT 6.0 wind turbine, which has a capacity of six megawatts, and our B75 rotor blades, which, at 75 meters in length, are the longest blades of their kind currently in operation wordwide. And although Jens Hald Jensen has worked in the wind industry ever since earning his university degree, he sees this test as the highlight of his career to date. “It’s simply incredible to stand here between these gigantic rotor blades – just look at these unbelievable dimensions,” exclaims the engineer from the Danish town of Brande. “It really is a technical tour de force to be able to manufacture something this imposing in one piece.”
More than just an impressive rotor For decades, Jensen has dreamed of an energy infrastructure that relies more heavily on renewable sources such as wind. “The wind delivers an unbelievable amount of energy around the clock, especially offshore,” says the engineer enthusiastically. “The transition to a new energy system is offering us the opportunity to help shape the future of energy – and that’s where I feel a very personal responsibility to future generations.”
It’s no wonder that Jensen is excited about combining the SWT 6.0 turbine with the B75 rotor blade: a single turbine will be able to supply green energy to 6,000 European households – emission-free and without the use of fossil fuels. And the first customers are already lining up to make large-scale use of the new technology: plans call for installing 300 SWT 6.0 turbines with a total capacity of 1,800 megawatts off the coast of the UK between 2014 and 2017.
LEFT – The housing – or “nacelle” – for the generating components of the Siemens SWT 6.0 gearless wind turbine is 15 meters long and 6.5 meters wide.
Years of offshore experienceOnce the turbines and rotor blades have successfully completed the test phase, two giant cranes lift the housing for the SWT 6.0’s generating components into the air. Under Jensen’s watchful eye, the housing – or the “nacelle” – is moved in slow motion to the top of the 120-meter tower. The culmination of more than 20 years of experience in offshore projects, the SWT 6.0 is remarkable not only for its output but also for its new drive technology, which is entirely gearless. Such innovations have enabled our engineers to reduce the number of components by about 50%. The streamlined design facilitates maintenance while also cutting down on weight: the SWT 6.0 is by far the lightest wind turbine in its class. And this, in turn, lowers costs for the foundation and the tower – making wind energy more competitive and moving us a step closer to Jensen’s vision of a greener energy future.
ABOVE – Once installed, the gigantic rotor will sweep an area equivalent to two-and-a-half soccer fields. An enormous amount of space is also required for unloading the rotor blades and mounting them on the hub (pictured on the left).
The largest single-cast fiberglass componentBut Jens Hald Jensen has no time for visions today. Because once the turbine is assembled, it’s time to hoist up the three giant rotor blades with steel cables. “This is the biggest rotor blade we’ve ever installed,” notes Jensen. “It’s a monumental challenge to hoist up the blades – which have a total rotor diameter of 154 meters – and attach them to the turbine.” Each rotor blade looks a bit like a beached whale, and people standing beside it look as small as they would next to one of the giant creatures of the sea. After all, the B75 is the largest single-cast fiberglass component ever constructed. And it’s innovations like this one that Jensen always finds exciting. “Our intense involvement in this field demonstrates very clearly that we intend to be pioneers in shaping the future of energy,” he says during a break. “The products shown here in Østerild underscore our commitment to leadership.”
Dr. Felix Ferlemann, CEO, Siemens Wind Power “Every second that the rotor, which has a total diameter of 154 meters, operates at a wind speed of ten meters per second, it captures the energy of 200 metric tons of air.”Our technologies are bringing the future of energy closerSiemens offers its customers not only wind power installations but also a broad portfolio of other products and solutions that will facilitate the transition to a new energy infrastructure: long-distance low-loss high-voltage direct-current transmission systems, components for the smart grid of the future, gas turbines with record efficiencies, and high-efficiency electric motors that cut energy consumption. Only an integrated technology company with a broad portfolio can provide such a complete range of offerings – thus strengthening public confidence that the transition to a new energy system can indeed be achieved. Because rebuilding our energy infrastructure will require much more than “just” phasing out nuclear energy. Many individual innovations along the entire energy chain will have to fit together perfectly like the pieces of a puzzle in order to make tomorrow’s energy supply both reliable and sustainable. And it’s here that our Environmental Portfolio is equipping us to play a key role.
In Østerild, we’ve just taken another step forward. After hours of exacting work, two crane operators and a handful of our technicians have attached the three rotor blades to the wind turbine. Jens Hald Jensen looks up with rapt attention, captivated by the imposing sight. “These rotor blades have a very special magic for me,” he says pensively. “I saw them while they were still on the ground, I was there when they were raised up, and now I’m watching them rotate and produce energy – it’s simply magical.” Nothing more stands in the way of the exhaustive testing that will follow in the weeks ahead. But for now, Jensen has called it a day. “We did it!” he exclaims, making no attempt to hide his feelings. “We’ve just installed one of the world’s largest wind turbine rotors – now that’s something you just have to be proud of.”
ABOVE – A job well done: after two huge cranes have positioned the rotor – which has a total diameter of 154 meters – specialists connect it directly to the generator shaft.
RIGHT – Smiles all around following the successful assembly of the wind turbine: Dr. Felix Ferlemann, CEO of Siemens Wind Power (center), and Jens Hald Jensen, project manager in Østerild (back right), share a proud moment with colleagues.
“Building a new energy system is a huge challenge.”
Providing energy for the future will require innovative solutions and strong partnerships. Siemens and the energy company Energie Baden-Württemberg AG (EnBW) have been cooperating closely for years. Dr. Hans-Josef Zimmer, Chief Technology Officer of EnBW, talks about the steps that must be taken to usher in a new energy era.
Dr. Zimmer, the future of energy is currently a hot topic in Germany. What stance is EnBW taking?
Dr. Zimmer: Building a new energy system is a huge challenge for Germany. And as one of the country’s largest energy companies, we’re tackling it head-on. In terms of our strategy, this means we’re continuing to safeguard our position as a low-carbon energy producer. In addition to supplying power from highly efficient conventional plants, we intend to double the amount of power we generate from renewable energies by 2020. We already have a relatively large share of hydropower-based renewables in our portfolio. By 2020, we want to further expand our installed capacity from renewables by about 3,000 megawatts.
One step in this direction is certainly the EnBW Baltic 1 wind farm, Germany’s first commercial offshore wind installation. Your company partnered with us on its construction in 2011. How did the idea for this project develop, and what conclusions have you drawn from the operation of the wind farm?
Dr. Zimmer: We on EnBW’s executive board decided in fiscal 2007/2008 that we wanted to invest more heavily in renewable energies. Complementing our traditionally strong involvement in hydropower, we’ve defined wind energy as a further focus. Following extensive analyses, we concluded that wind turbines and wind farms, both onshore and offshore, could be particularly profitable. That’s why in 2008 we bought four licenses for offshore installations – two in the Baltic Sea and two in the North Sea – and now we’re in the process of developing these projects. The EnBW Baltic 1 wind farm has 21 wind turbines from Siemens and a total capacity of up to 48.3 megawatts. We’re very satisfied with its current performance. Availability is very good, and we achieved quite gratifying overall results the first year.
How’s the partnership with Siemens worked out?
Dr. Zimmer: When planning and implementing projects of this magnitude, we need reliable partners who keep their promises. Since the very beginning of the EnBW Baltic 1 project, the cooperation with our colleagues at Siemens has been characterized by great trust. And this trust is also based on our experience in other major projects on which we have partnered.
EnBW Baltic 1 is quite far from your home region in southwestern Germany. How is the electricity generated there distributed throughout the country?
Dr. Zimmer: Our wind farm in the Baltic feeds directly into the 50-hertz grid. From there, the energy is further distributed within Germany via an extensive interconnected grid. If we build more wind farms on the coast and offshore, where there’s lots of wind, we’ll have to transport large amounts of energy to the southern part of the country. By 2030, offshore wind farms operating off Germany’s coasts are expected to be supplying 25,000 megawatts of electricity. That’s why we’ll also need low-loss high-voltage direct-current (HVDC) transmission in the future. The grid development plan prepared by our subsidiary Transnet BW and three other grid operators foresees HVDC transmission lines along several corridors. However, I’m assuming the approval process will take a very long time. There are also technical challenges to be mastered – because, even though HVDC lines have already been installed in countries like China and India, that doesn’t mean such routes can be planned and implemented overnight in Germany. On the contrary, the process will take several years. But we must address this challenge if we want to succeed in restructuring the energy system.
LEFT – EnBW has commissioned Germany’s first commercial offshore wind farm, the EnBW Baltic 1 project, using wind turbines from Siemens. Comprising 21 turbines with a total capacity of 48.3 megawatts, the installation is located in the Baltic Sea, about 16 kilometers north of the German town of Zingst on the Darß peninsula.
In our view, highly efficient power plants like our combined cycle plants are another factor that can facilitate the transition to a new energy infrastructure: Stadtwerke Düsseldorf, a municipal utility in which EnBW holds a majority stake, plans to build just such a plant at the Lausward site in Düsseldorf. As with the EnBW Baltic 1 and 2 projects, Siemens will be the supplier. What criteria played a role in your investment decision?
Dr. Zimmer: Combined cycle power plants of the type supplied by Siemens are highly efficient systems that generate low-carbon power. They have fast-start capability and are highly flexible in terms of startup and shutdown – which makes them particularly suitable for an energy market moving toward fluctuating renewable energies. Of course, in addition to boasting high efficiency and rapid startup, every new plant must also be economically viable.
Another concern is reducing energy consumption, in other words, saving electricity. What can an energy company like EnBW contribute here?
Dr. Zimmer: A couple years ago, our slogan was “Empowered to cut consumption.“ Now you could, of course, say that a utility company should be happy if its customers use lots of energy. But quite the opposite is true: we want to help our customers conserve energy and boost energy efficiency. For years, we’ve been offering tailored solutions that make our customers’ operations more energy-efficient. One thing is clear to us: at EnBW, we can be competitive only if we provide our industry customers with energy that is so affordable that they can keep their production in Germany.
Smart grids are one option for flattening consumption peaks. To what extent is EnBW involved here?
Dr. Zimmer: We’ve been testing smart grids in trial communities for several years now. We’re also analyzing how our customers can benefit from intelligent electricity meters. We want to help our private, business and industry customers consume less energy. For example, appliances and equipment that require a lot of energy should be operated at night, when electricity is less expensive, rather during the day, when demand is high.
That sounds like a business field with lots of potential for EnBW. How can Siemens provide support here?
Dr. Zimmer: Siemens is a technology leader in many fields. Since the entire development process for the production, distribution and consumption of energy is extremely complex, system providers like Siemens have major market opportunities.
In your view, what factors are most crucial for the successful transition to a new energy system?
Dr. Zimmer: We need a wide range of technical solutions to make the new system a success. In addition, a very stable legal framework for marketing renewables must be in place. We also need to expand the grid so that energy from the generation centers, which in the future will be in northern Germany, can be transported to the consumption centers in the south. We’ll need a greater number of highly flexible power plants, such as the combined cycle plants I’ve already mentioned. In addition – and this is very important – we’ll need a public consensus to implement all of these things. Grid expansion will entail installing hundreds of kilometers of transmission lines all across Germany. And the construction of additional pumped-storage hydropower plants to store energy temporarily will also have an impact on the environment. We have to convince people and make it clear that the transition to a new energy system cannot be accomplished from one day to the next but will require a great deal of patience, money and effort.
LEFT – Plans are far advanced for the construction of the world’s most efficient natural gas power plant – an order placed by Stadtwerke Düsseldorf, a municipal utility in which EnBW holds a majority stake. Here EnBW Chief Technology Officer Hans-Josef Zimmer examines up-to-date project planning information from Siemens. The plant is expected to begin supplying ecofriendly electricity and district heating in 2016.
In which of these fields do you anticipate major advances?
Dr. Zimmer: We need highly efficient plants, but it will take time to develop them. After all, Siemens didn’t develop its high-efficiency combined cycle plants overnight. And we’ll also need time to install HVDC transmission lines and smart grids throughout Germany. Until that happens, coal-fired plants will also be a component of the evolving energy system. While such power plants will still be necessary as a backup for many decades to come, they’ll be more efficient than before, delivering the same output while consuming much less fuel.
Now you’ve brought up the topic of the energy mix. How will the energy mix at EnBW look ten years from now?
Dr. Zimmer: While EnBW will also still be operating conventional plants in ten years, we intend – compared to today – to double the share of renewables by 2020, expanding their capacity by about 3,000 megawatts. Renewable energy sources include offshore wind, onshore wind, photovoltaics, biogas and water. To obtain an economically viable mix, all types of renewable energies will have to be combined. That’s how the restructuring of the energy system will succeed.
What do you expect of Siemens in this context?
Dr. Zimmer: We expect that Siemens will always be at the cutting edge of technology and that we can count on Siemens as a technology leader who provides us with efficient solutions – solutions that make sense from both an economic and an environmental perspective. We value Siemens’ power of innovation. And we value the trust that we have in Siemens, which has evolved over many decades, just like the plants that we built together and are successfully operating today. We expect Siemens to continue pursuing this strategy and to offer us the best solutions on the market. And we at EnBW wish Siemens every success in this endeavor.
We’re convinced that the transition to a new energy system will succeed. It will unleash a wave of innovation and create an exemplary energy infrastructure. Our technologies are making it possible to increase the share of renewables in the energy mix and slash greenhouse gas emissions. To make the transition a success, a variety of measures will have to be implemented – measures that fit together like the pieces of a puzzle. Here are some examples of how our technologies are already shaping the future of energy.